TIDUC07 March 2022
One important factor when designing an angle encoder using these devices is the actual sensor location on the PCB. The sensor placement in the package may result with unintentional placement errors in any of the 3 axes.
DRV5055 has the benefit that the sensor location in the XY plane is centered relative to the package. However, the implementation for this device requires two sensors placed 90° separated about the magnet. Additionally, it may be necessary to use an LPG through-hole package depending on the sensor location.
For TMAG5170, the layout files TIDA-060040 contain an alignment layer which indicates the actual sensor location. Additionally, a via has been placed at the target sensor location to assist with alignment.