TIDUC26A April 2022 – April 2024
The differences shown between the buttons is due to more than just the material difference. Because these test units were hand assembled, there is variation in the mechanical alignment and the adhesion that creates the mechanical isolation. This difference can cause some of the buttons to have a worse response and can be alleviated by having a controlled and repeatable assembly process. The different force responses can be offset by applying a different gain factor to each button so they all end with a button output at the same force. To better showcase this, the raw data is collected for each button with varying forces. The force response for the ABS button surface is shown in Figure 3-3.
(a) Left Side | (b) Right Side |