TIDUC26A April 2022 – April 2024
Since the LDC3114 uses the same I2C address, an I2C MUX is used to communicate with each device independently. Each LDC3114 is driving four sensor coils at the default 40SPS. Since touch buttons do not require high-speed operation, the sample rate does not need to be increased and polling each device for data does not cause a latency issue on the touch button. For battery powered applications, the sample rate can be decreased and the digital outputs of the LDC3114 can be monitored instead of using the I2C data. In this design, there were limited GPIO ports on the connector to the main controller so the digital outputs are read from the OUT register of each device instead.