By connecting 27.4-kΩ resistor on
MODE/S-CONF pin, the device is configured to:
- VSET operation: VOUT is
sensed only through the VOS pin by an internal resistor divider. The target
output voltage is programmed by an external resistor connected between the
FB/VSET pin and GND. In this design, FB/VSET pin is floating and thus the VOUT
is programmed to 3.3-V
- 2.5-MHz Switching Frequency
with AEE (Automatic Efficiency Enhancement): The MODE/S-CONF pin is
configured to AEE mode which provides efficiency enhancement over the entire
input voltage and output voltage range by automatically adjusting the switching
frequency of the converter. The efficiency decreases if VOUT decreases, VIN
increases, or both. To keep the efficiency high over the entire duty cycle range
(VOUT/VIN ratio), the switching frequency is adjusted while maintaining the
ripple current. The AEE feature provides an efficiency enhancement for various
duty cycle, especially for lower VOUT values where fixed frequency converters
suffer from a significant efficiency drop. Furthermore, this feature compensates
for the very small duty cycle of high VIN to low VOUT conversion, which limits
the control range in other topology.
- Power Save Mode Operation(Auto
PFM/PWM): The MODE/S-CONF pin is configured for power save mode(Auto
PFM/PWM). The device operates in PWM mode as long as the output current is
higher than half of the ripple current of the inductor. To maintain high
efficiency at light loads, the device enters power save mode at the boundary to
discontinuous conduction mode (DCM). This happens if the output current becomes
smaller than half of the ripple current of the inductor. The power save mode is
entered seamlessly when the load current decreases. This ensures a high
efficiency in light load operation. The device remains in power save mode as
long as the inductor current is discontinuous. In power save mode, the switching
frequency decreases linearly with the load current maintaining high efficiency.
The transition in and out of power save mode is seamless in both
directions.
- Output Discharge Function
Enabled: The output discharge function is enabled to ensure a defined
down-ramp of the output voltage when the device is being disabled but also to
keep the output voltage close to 0-V when the device is off. The output
discharge feature is only active once TPS629210-Q1 have been enabled at least
once since the supply voltage is applied.