TIDUC65 April 2022 TPSI3050 , TPSI3050-Q1 , TPSI3052 , TPSI3052-Q1
Figure 3-2 shows when the load current (ILOAD) is greater or equal to 2 A and the design implements a delay of at least 100 ms before disconnecting the load. From the scope capture taken, it can be observed that the delay is larger than 100 ms. This is because the negative swing threshold from the AND gate can vary from 0.9 V to 2.2 V. The max value of 2.2 V was chosen for the calculation to ensure that the delay is greater or equal to 100 ms.
Figure 3-3 shows the behavior of the circuit when a current greater than 5 A is detected. The current load increases above 5 A and the overcurrent protection disconnects the load with a minimal propagation delay of 6.3 µs.
Figure 3-4 shows the visual warning using a red LED when the temperature reaches 60 °C. Figure 3-5 and Figure 3-6 are thermal images taken for the two temperature protection levels. When temperature is between 60 °C to 90 °C a visual warning is provided via a red LED and when temperature is above 90 °C the load is disconnected.