TIDUCL0 January 2017
In the conduction phase, the FETs are continuously conducting. The main parameter that affects current sharing during this phase is the RDS_ON of the FET. If RDS_ON of the FETs are not equal, then the FET with the highest on resistance carries the least current and the one with lowest on resistance carries the highest current. Because MOSFETs have a positive temperature coefficient of on resistance, the current sharing gets self-regulated. The FET carrying the highest current has the most conduction losses; this leads to temperature increase of the FET. Increased FET temperature causes an increase in the RDS_ON of the FET, which in turn reduces the current through the FET. This self-regulating mechanism makes the current through each FET close to each other over time.