TIDUCL0 January 2017
Figure 31 shows the motor winding current and winding voltage waveforms at a 18-V DC input and a 33-ARMS winding current. The result is tabulated in Table 5. The testing is done at 100% duty cycle. Figure 32 shows the steady state thermal image of the board at the same condition, captured after 10 minutes of continuous running. The maximum FET temperature observed is 87.9°C.
VDC (V) | IDC (A) | WINDING CURRENT (RMS) (A) | DUTY CYCLE | INPUT POWER (W) |
---|---|---|---|---|
18 | 38 | 33 | 100% | 680 |
Figure 33 shows the motor winding current and winding voltage waveforms at a 18-V DC input and a 31.8-ARMS winding current. The result is tabulated in Table 6. The testing is done at 90% duty cycle. Figure 34 shows the steady state thermal image of the board at the same condition, captured after 10 minutes of continuous running. The maximum FET temperature observed is 88.9°C.
VDC (V) | IDC (A) | WINDING CURRENT (RMS) (A) | DUTY CYCLE | INPUT POWER (W) |
---|---|---|---|---|
18 | 33 | 31.8 | 90% | 594 |