7.2.1.2 Switching Phase
The current sharing during the switching phase of the FET is affected by asymmetries in the gate drive circuit, differences in the circuit parasitics, and variations in device parameters such as transconductance gFS, threshold voltage VTH, and the input capacitances CGD and CGS. The effects of each parameter on current sharing are as follows:
- In order for all the FETs to be turned on at the same time, the gate drive circuit for each FET has to be very similar. The gate charge current for each parallel FET has to be equal. The gate voltage applied by the gate driver must be the same. Also there should be no skew in the gate-to-source voltages applied to the different FETs. If all these parameters are kept within a tight tolerance, the dynamic load current sharing of the paralleled FETs remains equal. One way to keep all these parameters in tight tolerance is to use a single gate driver IC to drive all the parallel FETs. This ensures minimal skew between the VGS of FETs and the VGS voltage remains the same. The gate current into each FET can be maintained close to each other by choosing gate resistor values that have a tight tolerance. The gate path impedance has to be kept same in routing and this is possible by use of the miniature power blocks.
- Circuit parasitics like the source (LS) and drain (LD) inductances affect the turnon and turnoff times of the FET. If one FET has a higher LS compared to the others, a higher voltage is induced across LS when current flows through it. This reduces the effective VGS applied to the FET, which in turn slows down the turnon time of the FET effecting dynamic current sharing. One solution to this is by making the layout symmetric so that the LS and LD of each of the FETs are close to each other. Matching LS and LD also ensures that the rise and fall times of current in each FET is close.
- The threshold voltage of FETs is another important parameter affecting current sharing. The FET having the lowest VTH turns on first and carries the highest current. Therefore, the FETs selected should have a tight tolerance in VTH. Usually the FETs from one production batch have VTH close enough that by the time the current through one FET rises significantly, the gate voltage of other FETs reach their VTH reasonably quick and start conducting. Also, it is important to have individual gate resistances for each of the FET. If individual gate resistances are absent and all the gates are shorted together, then the FET—which reaches its VTH first—goes into the Miller region faster and clamps the gate of the other FETs to its Miller voltage, which further slows down the gate voltages of the remaining FETs. This significantly effects the turn on behavior. VTH is also dependent on temperature. The higher the temperature, the lower the VTH; this ensures that the FET turns on even faster, which may lead to runaway conditions. Therefore, it is important to maintain all the FETs at equal temperature. Distributing the heat in the PCB by extending the copper planes helps here.
- Transconductance gFS of the FET also affects the dynamic current sharing between the FETs. The FET with the highest gFS has a faster rate of change of drain current with change in the gate-to-source voltage. So, during turnon, the FET with the highest gFS conducts the most current, and during turnoff the FET with the lowest gFS conducts current for a longer time.
- The input gate-to-source capacitance CGS and gate-to-drain capacitance CGD also affect dynamic current sharing. If the gate drive for all the FETs is symmetric (that is, drive voltages and currents are equal), then the FET with the lowest input capacitance CISS reaches its threshold voltage first and conducts the most current during turnon. During turnoff, the FET with the highest input capacitance reaches its threshold voltage last and conducts current for a longer time. To reduce the impact of the input capacitance on current sharing, it is important to use individual gate resistors with low values.
Using low values ensures that all the FETs with variations in CISS reach their threshold values fairly close to each other. Selecting gate resistors is a trade-off between suppressing circulating currents and suppressing the effect of variations in CISS and VTH.