TIDUCU8A september 2022 – may 2023
Other than the IO-Link physical layer tests, also the integrated current sink is tested. Figure 3-7 shows the current into the CQ line, when only the RX together with the current sink is active. With a current of about 8.5 mA it is well within the allowed range of 5 – 15 mA.