Make sure the hardware is setup as outlined in Figure 3-20. Do not supply any HV power yet to the board.
powerSUITE Settings : On the powerSUITE page select under Project Options section:
Select Lab 4 under Lab option.
Also disable the other options such as Non Linear Voltage Loop, Adaptive Deadtime and Phase shedding
Assuming all other options are same as specified earlier in Section 3.1.2.5.1.1
Under Control Loop Design, select Tuning as Voltage Loop. Style presets to DCL PI_C3 Save the page by Ctrl + S, and click on the Compensation Designer button ().
Make sure the load connected at the output of the board is correctly entered on the powerSUITE cfg page because this load value is used in the design of the voltage compensator.