TIDUD61E October 2020 – April 2021
This feature can be turned off or on by writing to the TTPLPFC_INPUT_CAP_COMPENSATION #define variable in the <solution>_user_settings.h file. This setting can be modified by the user. The value of the adjustment is controlled using the #defines TTPLPFC_HIGH_LINE_INPUT_CAP_COMP_ADJUST & TTPLPFC_LOW_LINE_INPUT_CAP_COMP_ADJUST. These are in per-unit format and how this value is determined was explained earlier in this section.
#define TTPLPFC_INPUT_CAP_COMPENSATION 1
#define TTPLPFC_HIGH_LINE_INPUT_CAP_COMP_ADJUST -0.02
#define TTPLPFC_LOW_LINE_INPUT_CAP_COMP_ADJUST -0.01