TIDUD61E October 2020 – April 2021
In this lab, the inner current loop is closed that is the inductor current is controlled using a current compensator Gi. Both DC bus and output voltage feedforward are applied to the output of this current compensator to generate the duty cycle of the inverter along with soft start for PWM around the zero crossing The current loop model is identical to PFC mode operation shown in Section 3.1.2.5.2 except for the direction of the reference current.