Figure 3-1 shows the TIDA-010242
board.
This sections shows how to setup the
TIDA-010242 for testing.
- Power Supply Input - Connect the
input power to J1 and J3 (SGND). The nominal power supply is 28 V and put the current
limit for the power supply at 5 A.
- Enable Jumper - Place a shunt
across pin 1 and 2 of J2 to enable the device. A shunt across 2 and 3 or the shunt is DNP
disables the LM7480-Q1.
- Power Output - The output power
can be measured or connected to via J4 and J5 (SGND). These jumpers can also be used to
connect to a electronic load for load testing.