3.1.2.1 Software Loading for TIDA-01580 Board (Transmit Side of BLE)
Plug in the LAUNCHXL-CC2640R2 board on the USB port of the PC. See the setup in Figure 3-9 and Figure 3-10. Table 3-1 lists the connections between the TIDA-01580 board and the LAUNCHXL-CC2640R2 board.
Figure 3-9 Programming TIDA-01580 Board Using LAUNCHXL-CC2640R2
Insert one CR3032 battery into the BT1 connector on the TIDA-01580 board, and power it on by using the S2 switch (ensure J8 is shorted on the TIDA-01580 board).
Open CCS as administrator (Right click on the CCS icon and run as administrator).
Click on the Project option in the main toolbar and then click Import CCS projects.
Browse to select the installed firmware (Default: C:\Program Files (x86)\Texas Instruments\TIDA-01580\TIDA-01580_firmware) and import all projects. Click the OK button.
Click View, Project Explorer and select TIDA-01580_firmware_tx.
Click on the Run and Debug buttons. This action programs the board with the selected project file.
Disconnect the TIDA-01580 board from the LAUNCHXL-CC2640R2 device.
Figure 3-10 Connections Between TIDA-01580 Board and LAUNCHXL-CC2640R2
Table 3-1 Connections for Programming TIDA-01580 Using LAUNCHXL-CC2640R2
CONNECTION ON LAUNCHXL-CC2640R2 (ON XDS110 OUTSIDE)