TIDUDT0 September 2022
The TPSM5D1806 is a module that can either be dual 6-A converters, or a single 12-A multiphase converter. Furthermore, because the TPSM5D1806 is a module, the overall solution size is relatively small for the power output it is capable of providing. The TPSM5D1806 is used for higher current accessory rails, system rails, and is used to provide the 5-V intermediate rail needed by the TPS650861 converters.