TIDUE90 July 2018
It is critical to design the user interface to work reliably under all expected environments. Unlike a mechanical button that uses physical movement to trigger a touch event, a capacitive touch button is fundamentally different. It triggers a touch event by detecting the changes in the electric field and capacitance of the sensors over time. Unfortunately, this operating principle makes capacitive touch buttons more vulnerable to influence by liquids. The changes in the electric field and capacitance of the sensors can be due to human interaction, such as a finger or hand, but the human body is not the only thing that can affect the electric field and capacitance. Water and other liquids on the touch surface can also create changes to the electric field and capacitance similar to the changes causes by the human body. The changes caused by the presence of liquids result in the false touch detections or inaccurate touch detections.
Different end equipment can have different requirements for handling detection when liquids are present. For some products, the user interface is designed to reject any touch events if there is liquid covering the touch surface. For other products, the user interface needs to accurately detect a touch event even when liquid covers the touch surface.