TIDUE90 July 2018
In addition to the design considerations that are discussed in this document, other factors must also be taken into account when designing a liquid-tolerant capacitive touch system.
For example, some applications require the capacitive touch system to work properly with liquid present while the user wears gloves to touch the panel. In these cases, the designer must define the expected use conditions and also to consider the tradeoff between responsiveness to gloved fingers and liquid-tolerant performance. The material, structure, and thickness of the glove can significantly affect capacitive touch performance parameters (such as sensitivity). The different capacitive sensing methods (self and mutual) also behave slightly differently when gloves are used while touching the sensors.
Other common design considerations include:
Overall, it is critical for a product designer to consider typical use cases and system factors (such as the ones listed above) that can affect the capacitive touch performance. This document does not describe all of these factors. This reference design is configured to reliably detect bare-finger touch when exposed to a continuous stream of water and a 3-Vrms conductive noise coupling directly to the power supply while eliminating false touch detections.