TIDUEA0A March   2019  – September 2020

 

  1.   1
  2.   Description
  3.   Resources
  4.   Features
  5.   Applications
  6.   6
  7. 1System Description
    1. 1.1 Key System Specifications
  8. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
    3. 2.3 Highlighted Products
      1. 2.3.1 Device Recommendation
      2. 2.3.2 Digital Temperature Sensor - TMP117
      3. 2.3.3 Digital Temperature Sensor - TMP116
      4. 2.3.4 ESD Protection Devices
    4. 2.4 System Design Theory
      1. 2.4.1 PT100, PT500, PT1000 based Measurement in Heat Meters
      2. 2.4.2 TMP117 Configuration as Temperature Sensor
      3. 2.4.3 Digital RTD Solution Using TMP117
      4. 2.4.4 Ambient Temperature Considerations
  9. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Required Hardware and Software
      1. 3.1.1 Hardware
      2. 3.1.2 Interface Test Software for TMP116
    2. 3.2 Testing and Results
      1. 3.2.1 Test Setup for Performance Testing
      2. 3.2.2 EMI and EMC Test Requirements for DRTD
      3. 3.2.3 TMP117 EMI/EMC Test Results
      4. 3.2.4 TMP117 Based Temperature Probe Measurement Performance Test Results
      5. 3.2.5 TMP116 Based Temperature Probe Measurement Performance Test Results
      6. 3.2.6 I2C-bus Cable Length Considerations
      7. 3.2.7 Power Supply
      8. 3.2.8 ESD Test Results for TMP116
      9. 3.2.9 Summary
  10. 4Design Files
    1. 4.1 Schematics
    2. 4.2 Bill of Materials
    3. 4.3 Layout Prints
    4. 4.4 Altium Project
    5. 4.5 Gerber Files
    6. 4.6 Assembly Drawings
  11. 5Software Files
  12. 6Related Documentation
    1. 6.1 Trademarks
  13. 7About the Author
  14. 8Revision History

TMP116 Based Temperature Probe Measurement Performance Test Results

Similar to the TMP117 probe, our TMP116 DRTD probe was immersed into the precision Fluke oil bath with Galden HT200 oil. The temperature offset graph is shown in Figure 3-8.

TIDA-010002 TMP116 DRTD -20 to 130C Temp. Error DriftFigure 3-8 TMP116 DRTD -20 to 130C Temp. Error Drift

Note that the Class AA accuracy achieved with this TIDA-010002 DRTD unit without calibration is not guaranteed for all TMP116 devices by default.The DTRD probes using the TMP117 and TMP116 both achieve class AA accuracy and the offset values between the two probes are very similar as expected.

Similar to Section 3.2.4, respose time was measured in both stirred oil and still air. In Figure 3-9, the DUT has initial temperature of 20.5°C and is inserted into a 70°C hot oil bath and the DUT reported temperature has been logged. The response time in the oil bath between the TMP117 and TMP116 probes is very similar; it takes approximately 55 seconds for the probes to reach the oil temperature of 70°C.

TIDA-010002 TMP116 DRTD Response Time in Stirred Oil BathFigure 3-9 TMP116 DRTD Response Time in Stirred Oil Bath

The still air response time of two DRTD probes, named DUT1 and DUT2, is shown in Figure 3-10 and also compared to other TI test boards with the TMP116 thermal pad either soldered or not soldered. Obviously, the DRTD probes with their metal sheath and much larger thermal mass have a longer response time but after a delay of approximately 400 seconds they are equal to a bare PCB with TMP116. TP means Thermal Pad and tests have been made to compare the performance with and without soldering the thermal pad (for details see Precise Temperature Measurements with TMP116).

TIDA-010002 TMP116 DRTD Response Time in Still AirFigure 3-10 TMP116 DRTD Response Time in Still Air