TIDUEB8C July 2018 – March 2021 TPS274160
To get started, the two IO-Link master boards have to be stacked together and have to be stacked to the AM437x IDK. A 24-V, 5-A power supply has to connected to J8 or J5. Jumpers J6, J7, and J9 on the adapter board have to be shorted. In Figure 3-1 the related jumpers and connectors are shown. The LEDs for 24 V and 3.3 V should light up, when the corresponding voltage is present. In normal operation both LEDs will light.