TIDUED6B august 2018 – april 2023
When the collector node USB is connected to the PC, the device manager should recognize the following COM ports:
Launch TeraTerm, select "Serial" and select the XDS110 Class Application/User UART COM port from the drop-down menu and click the OK button. Verify that the COM port has the settings as Figure 3-17 shows.
A TeraTerm macro is included to parse the output of the collector node. To launch the macro, select Control menu, then select Macro option. Navigate to the TIDA-010022 firmware folder and select mmWave_collector_macro.ttl.