TIDUED6B august   2018  – april 2023

 

  1.   Description
  2.   Resources
  3.   Features
  4.   Applications
  5.   Design Images
  6. 1System Description
    1. 1.1 Key System Specifications
  7. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
      1. 2.2.1 mmWave Sensor
        1. 2.2.1.1 mmWave Sensor People Counting
        2. 2.2.1.2 IWR6843 UART Communication
          1. 2.2.1.2.1 IWR6843 Frame Output
          2. 2.2.1.2.2 IWR6843 Frame Header
          3. 2.2.1.2.3 TLV Elements
      2. 2.2.2 Power Supply Design
      3. 2.2.3 Wireless Network Design
      4. 2.2.4 CC1352 Software Design
        1. 2.2.4.1 Collector Node
        2. 2.2.4.2 Sensor Node
        3. 2.2.4.3 mmWave Sensor Configuration Command List Modification
    3. 2.3 Highlighted Products
      1. 2.3.1 IWR6843: Single-Chip 60- to 64-GHz mmWave Sensor
      2. 2.3.2 CC1352R: SimpleLink High-Performance Dual-Band Wireless MCU
      3. 2.3.3 IWR6843ISK and MMWAVEICBOOST: mmWave EVMs
      4. 2.3.4 LAUNCHXL-CC1352R1: SimpleLink™ Multi-Band CC1352R Wireless MCU LaunchPad™ Development Kit
  8. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Required Hardware and Software
      1. 3.1.1 Hardware Setup
      2. 3.1.2 Software Setup
        1. 3.1.2.1 Loading the CC1352 Firmware
        2. 3.1.2.2 Loading the IWR6843 Firmware
        3. 3.1.2.3 Starting the Firmware
        4. 3.1.2.4 Building the Firmware
        5. 3.1.2.5 Viewing Collector Data Output
        6. 3.1.2.6 Modifying the mmWave Configuration
    2. 3.2 Testing and Results
      1. 3.2.1 Test Setup
        1. 3.2.1.1 People Counting Setup
        2. 3.2.1.2 Power Consumption
        3. 3.2.1.3 Wireless RF Range
      2. 3.2.2 Test Results
        1. 3.2.2.1 People Counting Test Results
        2. 3.2.2.2 Power Characterization
        3. 3.2.2.3 Wireless RF Range Results
  9. 4Design Files
    1. 4.1 Schematics
    2. 4.2 Bill of Materials
    3. 4.3 PCB Layout Recommendations
    4. 4.4 Altium Project
    5. 4.5 Gerber Files
    6. 4.6 Assembly Drawings
  10. 5Software Files
  11. 6Related Documentation
  12. 7Trademarks
  13. 8About the Author
  14. 9Revision History

Loading the CC1352 Firmware

Follow these steps to load the firmware on the CC1352 LaunchPads:

  1. Download UniFlash from http://www.ti.com/tool/UNIFLASH.
  2. Open UniFlash and connect the sensor node and collector node to the PC.
    Note:

    See Section 3.1.1 for details on setting up the IWR6843 boards and CC1352 LaunchPad.

  3. Once the CC1352 is plugged into the PC, UniFlash will detect each individual device.
    Note:

    Both the 5-V power supply and a USB cable are needed to program the sensor node, but only the USB cable is needed to program the collector node.

  4. Highlight the device to be programmed and click the Start button.
  5. In the Program section, under Flash Image(s), click the Browse button.
    1. If loading firmware for the collector, navigate to the TIDA-010022 firmware folder and select the collector_cc1352r1lp.out file.
    2. If loading firmware for the sensor, navigate to the TIDA-010022 firmware folder and select the sensor_cc1352r1lp.out file.
  6. After selecting the correct image file, click the Load Image button.
  7. If the image was loaded successfully, the message "[SUCCESS] Program Load load completed successfully" is displayed.
GUID-1FBF1C03-2E67-4E3D-840D-6D1B3BE65D49-low.png Figure 3-5 Detected Devices
GUID-A111A465-603A-41F6-8687-122E089F8EF7-low.png Figure 3-6 Loading Image Successfully