The following figures show a possible set up from the reference design implementation. Images below are of the full TDA3x Automotive Starter Kit from D3 Engineering (note that SOM is not part of this reference design).
Note: Images shown are from the TDA3x Automotive Starter Kit.
- TDA3x system can be connected to a computer to access the debug Serial console. There is a USB Micro B connection, as shown in Figure 3-1.
- There is a Micro SD Card slot as shown in Figure 3-2.
- HDMI attached to a display to the TDA3x system in port labeled HDMI OUT, as shown in Figure 3-3.
- HDMI cable that is attached to a video source (for example, computer) to the TDA3x system in port labeled HDMI IN ,sa shown in Figure 3-4.
- Power to the TDA3x system, as shown in Figure 3-5.