TIDUEJ6A January 2019 – July 2022
The single-shot standard deviation of the differential ToF is a measure used to express the expected variance of the output at zero-flow and ambient temperature (see Figure 4-15). The STD is calculated by executing the application at an ambient temperature and in a zero-flow condition.
The MSP430 Ultrasonic Design Center GUI can then be used to capture the DToF for 5 to 30 minutes, and the STD can be calculated using a tool like MATLAB® or Excel®.
The single-shot STD of blocks of 200 measurements are computed and plotted in Figure 4-15. Each plot represents single-shot STD of 200 measurements. The plot shows that the variation of single-shot STD is approximately 20 ps, and the average is <400 ps.