TIDUEM7A April 2019 – February 2021
The MSP432 software used for evaluating this design is test software. Section 2.3.2.3 discusses the features of the test software, which provides insights on how to implement custom software for metrology testing. Subsequently, the metrology software is described as two major processes: the foreground process and background process.
The test data included in this reference design was taken using the generic test code. This test code has since been further developed into an energy metrology library software.
For all new designs, TI recommends using the ADC Energy Metrology Library software package. This software contains hardware abstraction layers which enable communication between an ADC and an Arm® Cortex®-Mx microprocessor (MCU), a library of metrology calculations for energy measurements, and electricity meter example application. The included polyphase electricity meter application was developed and tested on an Arm Cortex-M4 MSP432P microprocessor, but can also be ported to other microprocessors using the hardware abstraction layers. Also included is a Windows® PC GUI to display metrology parameters from the TIDA-010036 and TIDA-010037 reference designs.