TIDUES0E June 2019 – April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The UCC14141 device is selected as an isolated bias supply. This is a isolated bias module with an integrated transformer, offering the smallest footprint and height. The output is configured in a dual rail configuration to +15 V and –4 V. The maximum power drawn per device is calculated using the UCC14141-Q1 calculator tool available on the product folder. With this the value of the current-limiting resistor (RLim) (RLIM in Figure 3-11). Here 1 kΩ is selected for the devices only supplying one gate driver and 600 Ω is selected for the devices supplying one gate driver and the high side of the isolated sensing. Each output is connected to an LED indicating that isolated power is present. There are precautions on the board to share the isolated bias supply between the two low-side FETs on each side. For this jumper the resistors need to be placed and RLim needs to be adjusted. This is not tested yet. Additionally there is the option to populate a bootstrap supply for the high-side FETS, which is also not yet tested.