TIDUET3 February 2021
The total secondary-side RMS load current is the current referred from the primary-side current to the secondary side.
Because the secondary side of the transformer has a center-tapped configuration, this current is split equally into two transformer windings on the secondary side. The current of each winding is then calculated as:
The corresponding half-wave average current is: