TIDUET7G September 2019 – October 2023
Once the project is imported, the project explorer appears inside CCS as shown in Figure 3-21.
For this stage of this design <solution> is llc. The project structure is the same with ttplpfc in Section 3.1.2.2.
Double click the main.sysconfig file name in the project window. This GUI can be used to change the parameters for an adapted solution, like power rating, inductance, capacitance, sensing circuit parameters, and so forth.