powerSUITE settings: On the
powerSUITE page select under Project Options section:
Select Lab 4 under
Lab option
Also disable the other
options such as Non Linear Voltage Loop, Adaptive Deadtime
Assuming all other options are
same as specified earlier in Section 3.1.2.5.1.1.
Make sure the load connected at
the output of the board is correctly entered on the powerSUITE syscfg page
because this load value is used in the design of the voltage compensator.