TIDUET7G September 2019 – October 2023
Set the resonance point for the LLC converter close to 140 kHz to minimize the dimension of the LLC transformer set. The operating point of the LLC power stage is close to this frequency during a full load condition. Choose a value of Lr = 19 μH and Cr = 66 nF to calculate the value of the resonant frequency as follows:
A PQ 32/30 core has been used to realize the LLC transformer. The resonant inductance is provided through an additional shim inductor built on a 20/16 PQ core.