Install CCS from the Code Composer Studio (CCS) Integrated Development
Environment (IDE) tools folder, CCSV10.1 or above is recommended.
Install C2000Ware DigitalPower SDK at the C2000Ware Digital Power SDK
tools folder.
Note: powerSUITE is
installed with the SDK in the default install.
Go to View → Resource Explorer. Below the TI Resource Explorer, go
to C2000Ware DigitalPower SDK.
To open the reference design
software as it is (opens firmware as it was run on this design and hardware,
requires the board to be exactly the same as this reference
design).
Under C2000Ware DigitalPower SDK, select Development Kits → CCM
Totem Pole PFC TIDA-010062, and click on Run <Import>
Project.
These steps import the project, and the development kit or designs page show up.
This page can be used to browse all the information on the design including this
user guide, test reports, hardware design files, and so forth.
Click Import <device_name> Project.
This action imports the project into the workspace environment, and a
main.syscfg page with a GUI similar to Figure 3-3 shows up.