TIDUET7G September 2019 – October 2023
See the loading the custom bootloader and application to Flash using CCS section of the Live Firmware Update Reference Design with C2000™ Real-Time MCUs design guide for more information on how to import, build, and load the custom bootloader and application to Flash using CCS.
<C2000Ware_DigitalPower_SDK_path>\solutions\tida_010062\f28003x\examples\flash\CCS
Applicable build configurations include Bank0_LDFU and Bank1_LDFU.
Make sure that Bank0_LDFU is built before Bank1_LDFU. Once both build configurations are completed, proceed to the follow steps to the flash bootloader and application to the device.