The FSI is a serial peripheral capable
of reliable high-speed communication across isolation barriers.
- Make sure TTPLPFC_LAB in PFC
solution is set to 4 and LLC_AUTOSTART in LLC solution is set to 1.
- The primary side (PFC) MCU and
secondary side (LLC) MCU will continue to handshake until both MCUs recognize
each other. Once the handshake is completed, TTPLPFC_Handshake_Complete_Flag
should be 1. This is an inside background task. Check FsiRxARegs.RX_EVT_STS
registers in the primary and secondary side MCU if the flag is not 1.
- When the PFC output voltage
reaches 380 V, the primary MCU will automatically send a flush sequence together
with a ping frame to the secondary side MCU to start LLC. For more details of
flush sequence and ping frame, see the TMS320F28004x Real-Time
Microcontrollers Technical Reference Manual, TMS320F28003x Real-Time Microcontrollers Technical Reference
Manual, or TMS320F28002x Real-Time Microcontrollers Technical Reference
Manual.
Figure 3-33 shows the clock signal and data signal of flush sequence and ping frame waveform.
Figure 3-34 shows the clock signal and data signal of ping frame waveform.