Connect the GaN daughter cards
and C2000 Piccolo controlCard to the mother board as follows. The details of the
connections to each pin of the connectors can be found in the schematic of the
1-kW, 80+ Titanium AC/DC Power Supply Reference
Design.
One GaN daughter card 'LMG3410-HB-EVM' at connectors
Brd1 position
C2000 Piccolo controlCard
'TMDSCNCD280049C'/'TMDSCNCD280025C' at the connector J1 and J3
Connect the 3 Pins AC terminal of
reference board to the AC power source.
Connect output terminals with
wires to the electronic load, and maintain correct polarity.
Put a cooling FAN at the AC side
to keep the board in wind;
Set and maintain a small load of
approximately 10 A.
Current and voltage probes can be
connected to observe the input current, input voltage, and output voltages.