TIDUEW7 May 2020
There are two functional multi-purpose push buttons connected to GPIOs configured as inputs on the processor that can be used for software developers to test applications developed using this board. Three LED are connected to three GPIOs of the processor to indicate the status of processes that are running, completed, or may have failed. Both the push-buttons and status LEDs can be used for debugging or to provide tactile inputs and visual feedback to the user. These connections are shown in Figure 10.