TIDUEX2 July 2020
The design uses the adjustable output voltage version of TPS62088 which sets the output voltage of U2 and U3 depending of the value of the resistors R4, R6 and R7, R9 respectively.
The supply of the NAND IO is usually 1.2 V or 1.8 V. By default, U2 is set to output 1.2 V. However, it is also possible to use the IC fixed versions TPS6208812 or TPS6208818 to obtain 1.2 V or 1.8 V respectively. In that case, R4, R6 and C6 should be removed and the FB pin should be connected to the output. The difference in the design is shown in Figure 2-2 and Figure 2-3.