TIDUEX5 October 2020
Warm Start testing is performed to ensure the design functions as appropriate during a warm-start event. Warm Start sees a decrease in battery voltage resulting in the need to ensure the reverse current blocking feature works as intended. As shown in Figure 3-14, the DGATE pulls low when the output voltage is higher than the input voltage to make sure reverse current blocking takes place.