TIDUEY1B November 2020 – April 2024 BQ25798
To power on the TPS25750D device when the system needs to source power, the VIN_3V3 input pin must also be supplied. Therefore, the TLV75533 was chosen to provide the 3.3 V needed to power the PD controller. The input is connected to the TPS54531 output of 5 V, which drops down to 3.3 V. However, this input supply is not needed for sink-only applications and so the 3.3 V rail can be omitted as well if that is the case.