Use the following options when setting up the input reference signals:
- Option 1: The onboard reference LMK61E2 (U2) is
powered up using the jumper J16 and factory programmed to generate a 156-MHz
LVDS output. U2 can be programmed to generate different clock frequencies using
the I2C interface. The clocking board has a CDCLVP111-SP clock buffer (U9) to
select the reference input from U2 or external reference, Y1, and distribute to
the clocking devices on the board. U9 can select the LMK61E2 reference using the
short jumper at pin 2-3 of the jumper J30. Isolate the power supply to Y1 by
removing the short jumper at J8.
- Option 2: Connect the external reference signal to the OSCin_P and OSCin_N connectors. While connecting the external reference, power down the Y1 by removing the short jumper at J8 and remove C87. For external reference enable to clocking devices from reference buffer device U13, place the short jumper at pin 1-2 of J30. At the same time, isolate the power supply to U2 by removing the jumper J16.
- Option 3: The onboard VCXO Y1 is powered on using the jumper J8 and outputs a 100-MHz signal to the CLK0_P pin input of clock buffer (U9) by removing R39 and connect 50 Ω at OSCin_N connector. Place the short jumper at pin 1-2 of J30 and distribute the reference to clocking devices. At the same time, isolate the power supply to U2 by removing the jumper J16.
- Option 4: Use one of the previous options, when
LMK04832-SP works in single PLL mode (PLL2). When
LMK04832-SP is operating in distribution mode or
dual PLL mode, connect the external reference to
J6 or J10 or J5 depending on the operating input
frequencies. Next, choose between the LMH5401-SP
based active balun (U6) or onboard passive balun
(U40). Finally, select the path to CLKin1 pins of
the U1 by placing C79 and C80 or C38 and C3. While
operating in distribution mode, power down the Y1
by removing jumper J8. In distribution mode, when
the input frequency is higher than 3 GHz, then the
external clock input through the J5 connector can
be fed to Fin0 pins of the LMK04832-SP and connect
the external clock through R553 and R554 and
remove R555 and R556.