TIDUEY8 March 2023
For clock distribution there exist multiple potential topologies to get the primary clock to the individual clock devices and clock multipliers. Two of them are shown in the diagram Figure 2-4 as options A and B. In option A the primary clock is replicated in the system clock device and then fanned out into the individual multipliers. In option B the fan-out is done before the system clock and all clock devices and multipliers get their individual copy of the primary clock from there.
In this design option B was chosen because there the number of sequential stations in the clock path is smaller and less noise is expected from that.
For buffering the clock reference, the CDCLVP111-SP is an good choice because this device has all important parameters characterized and documented in the data sheet. From the various device alternatives, this device provides the lowest noise adder.
The reference design has also some provision for a purely passive clock distribution by using a 1:4 power splitter as shown in Figure 2-5. It is then possible to compare both designs. This comparison was not part of the measurements for this reference design.