TIDUEY8 March 2023
In this reference design the focus is in providing clocking and synchronization to two ADC12DJ3200QML-SP RF sampling ADCs, however, most systems typically have a need to provide clocking and synchronization to multiple high-speed data converters, in many instances a combination of many ADCs and DACs.
To scale the clocking tree for multichannel systems with more than two channels, consider a variety of clock architectures, such as a Tree or Daisy Chain configurations as illustrated in Figure 2-10.
In a daisy chain configuration, first the clocking board receives a high-frequency reference signal from an external clock source and generates the synchronized high-frequency clocks; then distributing the same reference signal to the next clocking board, along with the SYNC signals, to synchronize the two clocking boards. Conversely, in a clock tree configuration, one primary board (for example, LMK04832EVM-CVAL) receives a high-frequency reference signal from an external clock source, which is distributed to the secondary boards (clocking boards) along with the SYNC signals for synchronizing the secondary devices.
Examples of these configuration are shown in the following industrial-grade reference designs: