TIDUEY9 April 2021
The LP87702-Q1 device has programmable voltage monitoring for the BUCKx and BOOST converter output voltages and for VANA, VMON1 and VMON2 inputs. Monitoring of each signal is independently enabled in PGOOD_CTRL register. Voltage monitoring can be under-voltage monitoring only (PGOOD_WINDOW = 0) or
overvoltage and undervoltage monitoring (PGOOD_WINDOW = 1). This selection is common for all enabled monitoring. Enabled monitoring signals are combined to generate power-good (PG0, PG1) and/or interrupts as described in Power-Good Information to Interrupt and PG0 and PG1 Pins. Monitoring comparators have a dedicated reference and bias block, which is independent of the main reference and bias block.
In the AWR1843Boost EVM, the LP87702-Q1 handles the Voltage monitoring and has capability to enable the watchdog.
Watch needs to be enabled by writing into the WatchDog register in LP87702Q1 via I2C. For the watchdog operation the application firmware needs to generate a pulse every Window period on the GPIO(x). The recommended way to generate a pulse is to time the application and generate a pulse at appropriate points from the application in AWR1843. We do not recommend to use any timers in 1843 to generate this watchdog pulse.