The
following connections are required for programming (or updating) the software for
the wireless camera module:
- Connections between CC32xx
LaunchPad and wireless camera module (see Figure 3-2):
- UART TX
- UART RX
- GND
- Reset
- VSENSE (Level shifter
voltage)
- Reset Connection: For
proper operation of the OA7000, the Wi-Fi device should be able to reset it. To
do so, HOST_ON pin (pin 8, J7 connector) of the camera module is connected to
the NWP debug pin (pin 2, J13 connector) as shown in Figure 3-3.
- Optional connections required
for debug over JTAG
- JTAG (JTAG connector from
LaunchPad connected to the J5 connector of the camera module as shown
in Figure 3-4)
- nRESET
- GND
- Mount the sensor board on the
video processor board. Power up the camera using the battery connector (J1) or
using a micro-B USB as shown in Figure 3-5.