TIDUF01 November 2021 AWR2944
This reference design uses Doppler division multiple access (DDMA) processing where most of processing is done on the HWA and some intermediate tasks are offloaded to the DSP.
PARAMETER | SPECIFICATIONS | DETAILS |
---|---|---|
Maximum range (m) | 253 | This is the maximum range supported by the chirp configuration shown in Table 2-1. The maximum detectable range for a given object depends on the Radar cross section (RCS) of the object |
Range resolution (m) | 1.3 | The theoretical achievable resolution by AWR2944 is 3.75 cm based on 4 GHz bandwidth |
Maximum velocity (kmph) | ±143 | This is the native maximum velocity obtained after velocity disambiguation in DDMA. This specification can be improved by either using the range-rate in the tracker or higher-level algorithms |
Velocity resolution (kmph) | 0.37 | This parameter represents the capability of the radar sensor to distinguish between two or more objects at the same range but moving with different velocities |
Azimuth angular resolution (Deg) | 9.5 | This is the native azimuth angular resolution based on the virtual array aperture |