TIDUF03 December 2022
The design was tested from –40°C to 105°C, and measurements were taken at the output of the 4th order low-pass filter to measure output voltage versus fault current. The fault current input range was –10 mA to +10 mA. Figure 3-16 shows the output voltage of the active filters versus the fault current at different temperatures. The temperature drift is at a worst case of ±0.8 mA.