TIDUF04 December 2022
In normal use cases, high-current relays or contactors can typically draw 10s to 100s of milliamps as an inductive load, requiring specific drive architectures. Because of the amount of time that a relay or contactor requires to remain powered, an efficient drive solution is preferred to avoid thermal problems.