TIDUF06 August 2022
I2C communication between the DS90UB954-Q1 EVM and IMX623 imager over the FPD-Link III back channel can be confirmed with the Analog LaunchPad GUI. Figure 3-10 and Figure 3-11 show the established link with the serializer on RX port 0, and the corresponding register map.
Read and writes to the imager, at slave alias address 0x1A (7-bit), are confirmed with the built-in Python scripting window of the Analog LaunchPad. Register 0x8A54 reads data 0x1A, which is the expected default value for the register.