TIDUF06 August 2022
Once the FPD-Link III setup is done for the DS90UB953-Q1 and DS90UB954-Q1 devices, the I2C initialization can now be done on the IMX623. For these writes, see the IMX623 data sheet for register settings. There are many register settings listed to configure the imager, but as long as the DS90UB953-Q1 and DS90UB954-Q1 FPD-Link III parts are configured, the I2C back channel allows access to the IMX623 registers. For this testing, the IMX623 is configured for RAW12 output at 1920 × 1536 resolution and 30-fps.