TIDUF09 December 2022
This reference design incorporates three high-speed, high-current LDO's. When the reference design output is loaded with a high current, fast ramp rate load step, charge is transferred from the input supply through the LDO to the output. This rapid transfer of charge from VIN to VOUT can cause a significant voltage drop at VIN during the load transient. The LDO can momentarily enter dropout which will negatively affect the load transient performance. There are two common solutions:
The design engineer needs to carefully evaluate their load transient requirements and design the supply providing VIN accordingly to mitigate these concerns. This reference design has included a large capacitor bank to help with load transient evaluations using bench top power supplies. This capacitor bank might or might not be required in the final system based on the input power supplies performance.