TIDUF09 December 2022
This topology uses ballast resistors. Ballast resistors provide an easy way to connect multiple voltage sources together to supply power to a common load. It is critical to minimize the voltage difference at the output of each individual LDO. As LDO accuracy improves, the designer can reduce the size of the ballast resistor.
Each LDO has its own internal reference, which is slightly different than the other independent references. To achieve the smallest current sharing error between the different LDO's, this solution connects the current source reference's together through the REF pins. The remaining sources of error come from the ballast resistors, the internal output field-effect transistor (FET), and the amplifier. These errors show up as the offset voltage (VNR-VOUT) which itself is also a function of line and load. These sources of error make up the total error VE of each LDO. In this reference design the ballast resistors are configured to be the same value for simplicity.
Traditionally the ballast resistance was chosen using Equation 1 to set the current imbalance IMAX of the parallel LDO's. This formula does not account for the required load voltage, VLOAD, which is also a requirement for most modern power supplies designed with parallel LDO's. Texas Instruments has modernized the design and analysis of parallel LDO's using ballast resistors (see references [4] and [6]) and a down-loadable software tool has been developed to design RB for our LDO's and a set of system requirements (see reference [5]).
After RB has been selected, by using Equation 1, Equation 2 can be used to assess the current out of each LDO. Equation 3 can be used to assess the VLOAD of the system. For additional details on these equations, see reference [4]. Reference [5] can be used to quickly perform the calculations needed to select RB for a specified load current and load voltage.
Where:
In addition to IOUTn and VLOAD, other system requirements can require using a parallel LDO topology such as noise, PSRR, dropout and thermal limitations. In brief, parallel LDO's:
For a detailed discussion on all of these system requirements, how parallel LDO's can increase your performance, and how many parallel LDO's are needed for your system requirements, please see the references [4], [5], and [6].
Ballast resistors are typically employed as either a PCB trace or a discrete resistor. In general, PCB trace resistors favor applications which are low cost. PCB trace resistors also favor applications which operate in a narrow temperature range or experience very high temperatures. They are excellent choices where multiple low current devices are paralleled together (such as would be seen in high voltage LDO's which are usually limited in their available output currents). Discrete resistors favor applications which require maximum performance (where output voltage tolerance and transient responses are critical). Discrete resistors also favor applications where high current devices are being paralleled (such as low voltage LDO's where high current devices are readily available). Designing with a discrete ballast resistor becomes challenging when ambient temperatures exceed 125°C, and it is difficult to use discrete ballast resistors above 150°C. For a detailed discussion on ballast resistor analysis and design, see reference [4]
Ballast Resistor Option | Cost | Tolerance | Parasitic Inductance | High Temperature Operation |
---|---|---|---|---|
PCB Trace Resistor | Free after the PCB trace resistor design is complete. | Large: Resistor value nearly doubles across the operating temperature range. | Increases with PCB trace length | Only limited by the Tg of the FR4 |
Discrete Resistor | Must be sourced, purchased and installed on each PCB. | Low: discrete resistors come in 100 ppm or lower tolerances | Low | Large package sizes (0805 or 1206) can be required at higher temperatures. |