TIDUF15 March 2023
The PD controller in this reference design supports two channels, each having one downstream port (DS1 for first channel and DS2 for the second channel). This port acts as a device interface to connect the USB Type-C devices that negotiate the power and data from the PD controller. Both the ports are protected by the following ESD components.